Export Image

Associated with: WITS Firmware Images.

Security permission required to access this pick action: Configure.

You can use the Export Image action to export the firmware image file from Geo SCADA Expert. The firmware image file can then be used in external applications.

When you select Export Image, a browse window is displayed - select a suitable location for the export file and enter a suitable filename, and then select OK.


Disclaimer

Geo SCADA Expert 2019