Group Templates for Part of a Field Device's Configuration

You can use a Group Template to contain parts of a Field Device's configuration, rather than the entire configuration. For example, if you have multiple pumps in your system, you can create a Group Template for the points that are used to control and monitor an individual pump. You can then create Group Instances of that Group Template for each pump.

To use a Group Template to contain part of a Field Device's configuration:

  1. Identify the common elements in your system, for example, common types of pump.
  2. Log on to ViewX via a user account that has the Configure permission.
  3. Create a Group Template in your Geo SCADA Expert database (Select Create New and then select Group and then select Group Template. For more details, see Configure a Group Template).
  4. In the Group Template, create appropriate items for the common configuration elements. For example, you could add the points that are used to control and monitor a pump. For more details on configuring WITS items, please refer to the topics listed under Further Information (at the end of this procedure).
  5. Configure appropriate Property Overrides for the items in the Group Template (see Property Overrides).

    If your Group Template contains a WITS Outstation item, you need to configure a Property Override for the Outstation item's DocumentContent property. This property represents the bulk configuration file and each Outstation item (in the Group Instances) has to have its own bulk configuration.

  6. Repeat steps 3-5 for each common element of your system.

You have now completed the configuration of the Group Template(s) and can create Group Instances (see Configure a Group Instance).

To complete the configuration for your Field Devices, follow the procedure in the Pre-Configure Geo SCADA Expert - Upload or Import Later strategy. The only difference is that you will pre-configure by using a combination of 'ordinary' database items and Group Instances of Group Templates.

The Import or Upload process will be unsuccessful if any required Property Overrides are not in place for the Group Templates. It will also be unsuccessful if any of the points need to be converted to a different point type, for example, an analog input point may need to be converted into a minimum point.

Further Information

WITS Outstations: see Configuring a WITS Outstation

Configuring a WITS Analog Point

Configuring a WITS Binary Point

Configuring a WITS Counter Point

Configuring a WITS Firmware Image

Configuring a WITS Integrator Point

Configuring a WITS Maximum Point

Configuring a WITS Mean Point

Configuring a WITS Minimum Point

Configuring a WITS No Change Point

Configure a WITS Pulse (NULL) Action

Configure a WITS Pulse (Trip-Close) Action

Configuring a WITS Rate of Change Point

Configuring a WITS Runtime Point


Disclaimer

Geo SCADA Expert 2019