Minimum Configuration in Configuration Application, Load Into Field Device, Upload to Geo SCADA Expert

This strategy is appropriate if you want to use Geo SCADA Expert to undertake most of the Field Device configuration and you want to upload the configuration into Geo SCADA Expert.

Typically, you would choose to upload, rather than import, the minimum configuration into Geo SCADA Expert because:

If you decide to use this strategy, you will enter the minimum configuration in the Field Device's Configuration Application, load it into the Field Device, and then upload the configuration files into Geo SCADA Expert. You will then use Geo SCADA Expert to enter the incremental configuration settings (see Incremental Configuration File - Content and Syntax). Finally, you will download the configuration changes to the Field Device.

In the diagram below, BCF is the bulk configuration file and ICF is the incremental configuration file.

  1. Using the Field Device's Configuration Application, enter the minimum configuration (which includes defining the points for the Field Device and configuring the vendor-specific settings). Load the configuration into the Field Device. It can then be uploaded by Geo SCADA Expert.
  2. Log on to ViewX via a user account that has the Configure permission, and create and configure the Pre-Requisite Configuration for WITS Field Devices (WITS Device Profile, DNP3 Channel(s), DNP3 Outstation Set, WITS Outstation).
  3. In ViewX,upload the configuration from the Field Device into the Geo SCADA Expert database. (Right-click on the Outstation item that represents the Field Device, and then select the Upload Configuration action).

    The amount of time it takes for the upload to complete will vary depending on the type of Field Device and your communications infrastructure.

    When the upload is complete, Geo SCADA Expert uses the incremental configuration file to build the database. It creates points and profiles to match the configuration details in the incremental configuration file (see Automatic Creation of WITS Database Items). As you only made the minimum configuration settings in the Configuration Application, the incremental configuration file only contains the default settings.

  4. In ViewX, use the configuration Forms for the various WITS database items to apply the settings you require for your Field Device.

    For more information, please refer to the topics listed under Further Information (below).

  5. Download the configuration to the Field Device by using the Outstation item's Download Configuration (WITS Outstation) action.

Further Information

WITS Outstations: see Configuring a WITS Outstation

Configuring a WITS Application Program

Configuring a WITS Analog Point

Configuring a WITS Binary Point

Configuring a WITS Counter Point

Configuring a WITS Firmware Image

Configuring a WITS Integrator Point

Configuring a WITS Maximum Point

Configuring a WITS Mean Point

Configuring a WITS Minimum Point

Configuring a WITS No Change Point

Configure a WITS Pulse (NULL) Action

Configure a WITS Pulse (Trip-Close) Action

Configuring a WITS Rate of Change Point

Configuring a WITS Runtime Point

Configuring a WITS State Counter Point


Disclaimer

Geo SCADA Expert 2019