Pause

Associated with: WITS Application Programs.

Security permission required to access this pick action: Control.

The Pause pick action is only available for Field Devices that support the pausing and resuming of application programs. The device profile indicates whether the Field Device supports pausing and resuming ((see Display a WITS Device Profile)).

You use the Pause action to pause the execution of an application program that is running. You use the Resume action to resume the execution of a paused application program.


Disclaimer

Geo SCADA Expert 2019