Stop

Associated with: WITS Application Programs.

Security permission required to access this pick action: Control.

The Stop pick action is only available for Field Devices that support the stopping and starting of application programs. The device profile indicates whether the Field Device supports stopping and starting ((see Display a WITS Device Profile)).

You use the Stop pick action to stop the execution of an application program that is currently running. You can use the Start pick action to restart the execution of a stopped application.


Disclaimer

Geo SCADA Expert 2019