Trend Settings for WITS Mean Points

You can display the trend, or movement, of the value of a WITS Mean Point in the form of a graph.

The WITS Mean Point is a type of analog point. Therefore, many of the fields in the Trend section of the Mean tab are the same as those for other WITS analog points. The Maximum, Minimum andLogarithmic field values are inherited from the parent point (see Define an Analog Point's Trend Settings).


Disclaimer

Geo SCADA Expert 2019