WITS-Specific Status Descriptions on Historic Lists

You can display a Historic List for an individual point that has Historic Logging enabled (see Historic Lists in the Geo SCADA Expert Guide to Lists).

You use the Logged Data section of a WITS point’s configuration Form to specify whether Geo SCADA Expert should store Static (current) Data and/or Event (logged) Data historically for a WITS point (see Configure Logged Data Properties). You can subsequently display that data in the form of a Historic List. Each Historic List comprises a series of rows and columns.

The list's Status column may include both core and DNP3 status values for the WITS point, as well as the WITS-specific alarm/event inhibit status value ((see Status Attributes that are Common to Many Drivers) and (see DNP3 Driver-Specific <Update Type> Status Values) and see WITS Driver-Specific <Update Type> Status Values).

WITS-specific status values may also appear on point Status displays. For further information, see WITS Driver-Specific <Update Type> Status Values.

Geo SCADA Expert highlights the alarm/event inhibit status values with the 'Alarm Disabled' system color ((see Alarm Disabled)).


Disclaimer

Geo SCADA Expert 2019