Working with the Virtual ViewX Manager

The Virtual ViewX Manager is an application that is installed on each Virtual ViewX server machine. The application provides information about the server's communication settings, Virtual ViewX license, file locations, and so on.

This topic summarizes the information that is shown on each tab of the Server Manager window.

NOTICE

POTENTIAL LOSS OF COMMUNICATIONS OR SECURITY BREACH

Changing the settings on the Server Manager window without guidance from Schneider Electric support may result in the Virtual ViewX server being unable to run. It could also affect system security. Only alter such settings when advised to do so by Schneider Electric support.
Failure to follow these instructions can result in inoperable equipment or a security breach

To display the Server Manager window:

  1. In Windows, select the Start menu. Scroll down the alphabetical list of installed applications and expand the EcoStruxure Geo SCADA folder.

  2. Select the Virtual ViewX Manager option.
    With a Virtual ViewX server installation that is activated and licensed, the Server Manager Window is displayed - see below.
    (On new installations, the Product Registration Wizard is displayed - see License your Virtual ViewX Installation).

The Server Manager window contains various tabs, the contents of which are summarized below.

To close the Server Manager window, select the Close button.


Disclaimer

Geo SCADA Expert 2019