Connection Alarm

Associated with: Wonderware Historian database item.

The Connection Alarm attribute indicates the status of the network connection between HCAL and a Wonderware Historian server.

There are two types of connection error:

The Geo SCADA Expert alarm message includes any error message generated by HCAL.

Possible States: Displays one of the Geo SCADA Expert Standard Alarm States.

For information on resolving connection anomalies, see Troubleshooting Wonderware Historian Driver Operation.

Further Information

Connection State


Disclaimer

Geo SCADA Expert 2019