TagChannelStatus

Description

This is a value that indicates whether the tag value is late data or real-time data. If the property value is 0, then Wonderware Historian treats the tag value as late data. If the property value is 1, then Wonderware Historian treats the tag value as real-time data.

For more information, see the Wonderware Historian documentation.

Geo SCADA Expert Metadata Field

WH_TagChannelStatus

Default Value

The default value for this property is 0.

Type

Unsigned Word.


Disclaimer

Geo SCADA Expert 2019