TagDescription

Description

The description of the tag. The maximum length of the description is 512 characters. This property applies to all tag types.

Geo SCADA Expert Metadata Field

WH_TagDescription

Default Value

Class name and object ID. You can use the class name to determine what type of Geo SCADA Expert object is the source of the tag's data. You can use the object ID to identify which Geo SCADA Expert object is the source of tag's data. You can do this even if the object has been renamed and therefore the object name does not match the tag name (unless you have used the RenameTag method to realign the two names).

Examples: CDNP3AnalogIn,12345 or CPointAlgManual, 54321.

Type

String.

Further Information

Find a Wonderware Historian Tag's Source Point in Geo SCADA Expert.


Disclaimer

Geo SCADA Expert 2019