Wonderware Historian Driver-Specific Status Display Attributes

Every item in the Geo SCADA Expert database has its own Status display (also referred to as a View window or View dialog). You view an item's Status display by selecting that item's View Status pick action or menu option. The Status display provides information about the status of the selected item, presenting the information in the form of 'status attributes'. For further information about working with Status displays, see Status Displays.

Example:

The Status display for the Wonderware Historian database item provides information about:

  • The status of the network connection between Geo SCADA Expert and Wonderware Historian
  • The status of the store-and-forward cache (which temporarily stores export data if the network connection to Wonderware Historian is unavailable or intermittent).

The database items that are associated with this stand-alone driver support a combination of:

The driver first sets the status information when it uses HCAL to open a connection to the Wonderware Historian server. Thereafter, the driver polls HCAL every minute so that it can update the information if a status has changed. It also raises or clears alarms and logs events if required.

You can use the Refresh Status pick action to update the statuses immediately (that is, without waiting until the end of the current minute) (see Refresh Status)).


Disclaimer

Geo SCADA Expert 2019