Configure the Y-Axis Scale

You can specify the scale used on the y-axis. You do this using fields in the Y-Axis Properties window (see Configure the Y-Axis Properties).

Use the Scale section of the window to define these properties:


Disclaimer

Geo SCADA Expert 2019