Show or Hide a Trace's Markers

NOTICE

UNEXPECTED BEHAVIOR OF APPLICATION

You can hide a trace's content in Run or Design mode. If you are working in Design mode, ensure that the required trace content remains on show when saving the plot's configuration. Content that is hidden when the configuration is saved will continue to remain hidden from view by default.
Failure to follow these instructions can result in data being omitted from display unintentionally

You can show or hide a trace's markers. Hiding markers is useful if you only want to view the markers on a particular trace—you can hide the markers on other traces that overlap the trace in which you are interested.

To show or hide a trace's markers:

  1. Right-click on the tick (short line) that indicates the trace's position on the x-axis.
    A context-sensitive menu is displayed
  2. Select the Show option.
    A further context-sensitive menu is displayed.
  3. Enable or disable the Markers option as required.
    The trace's markers are shown or hidden depending whether you enabled or disabled the option.

There is also a Show>All option that you can use to show the trace, trace label, trace markers, and slice fill color associated with an individual trace. The Show>None option enables you to hide the trace, trace label, trace markers, and slice fill color associated with an individual trace (see Show or Hide the Whole Trace Entry).

Example:

An X-Y-Z Plot with markers and trace labels shown for each data source:

The same X-Y-Z Plot with markers hidden for the data sources other than 'Sensor 2'. (Additionally, the trace labels have been hidden for 'Sensor 3' and 'Sensor 5'.)


Disclaimer

Geo SCADA Expert 2019