Add a Dynacard Store

To add a Dynacard Store to the Geo SCADA Expert database:

  1. Display the Database Bar (see Display an Explorer Bar).
  2. In the Database Bar, right-click on the System or Group for which you want to add a Dynacard Store.
    A context-sensitive menu is displayed.
  3. Select the Create New option.
    A further menu is displayed.
  4. Select the Other option.
    A further menu is displayed.
  5. Select the Dynacard Store option.
    A Dynacard Store is added to the root of the System or to the selected Group (depending on your selection in step 2). It is selected automatically, ready for you to enter its name.
  6. Enter a suitable name for the Dynacard Store (taking into account the Geo SCADA Expert Naming Restrictions).
  7. Press the Enter key or select another part of the ViewX interface to confirm the entry.

When you have added a Dynacard Store to the Geo SCADA Expert database, you can then:

Once Geo SCADA Expert has uploaded dynacard data to the Dynacard Store, you can also Specify the Dynacard Data that is to be used as ‘Reference’ Data.


Disclaimer

Geo SCADA Expert 2020