Specify the Labels Used for the Dynagraph’s Axes

Use these fields on the Edit Dynagraph window to specify the text that is displayed for the axes’ labels:

X-Axis Label

Use to specify the text that is displayed alongside the horizontal x-axis, to indicate what information that axis represents. The default is ‘Position’. You can overtype the entry if required, or delete the field’s content if no label is required.

Y-Axis Label

Use to specify the text that is displayed alongside the vertical x-axis, to indicate what information that axis represents. The default is ‘Load’. You can overtype the entry if required, or delete the field’s content if no label is required.


Disclaimer

Geo SCADA Expert 2020