Define Advanced EWS Analog Point Scaling

Use the fields in the Scaling section of the Analog Point Tab to specify the type and range of the raw input signals, so that they can be suitably converted into floating-point engineering values for use in the Geo SCADA Expert database.

If the point is configured as an output point the settings in the Scaling section perform a similar conversion on any output signals. Geo SCADA Expert uses the conversion calculation to produce a raw data value that is sent to plant.

Use the following fields to configure the scaling settings:


Disclaimer

Geo SCADA Expert 2020