To add a User Roster:
- Right-click on the System or Group to which you want to add the roster (this might be a separate group for storing redirection actions, or for storing user details).
 A context sensitive menu is displayed.
- Select the Create New option.
 A further menu is displayed.
- Select the Alarm Redirection option.
 A further menu is displayed.
- Select the User Roster option.
 A User Roster is added to the system. It is selected automatically, ready for you to enter its name.
- Enter a suitable name for the User Roster (see Naming Restrictions in the Geo SCADA Expert Guide to Core Configuration).
- Select another part of the interface or press the ENTER key to confirm the entry.
When you have added a User Roster, you need to Configure the User Roster Properties.