Each database item that can generate alarms can be configured to have an Alarm View. An Alarm View is a ‘file object’, such as a Mimic, that can be used as an aid when an alarm is raised. You can configure Alarm Views on a per item or per Group basis (see Define an Alarm View in the Geo SCADA Expert Guide to Core Configuration).
Alarm views are displayed using the Display Alarm View pick action.