Why is Enable Alarms Having No Effect?

If the Enable Alarms action appears to be having no effect, it is probably because Geo SCADA Expert is using the Independent feature to prevent a potential conflict between users, Logic programs, Schedules, and Method Calls. At least one of the User Types is still disabling alarms for the item.

With Independent enabled, Geo SCADA Expert only stops withholding alarms for an item when there are no User Types disabling the item’s alarms (that is, all of the ‘Disable Alarms’ flags and the Overall ‘Disable Alarms’ state are 0).

Further Information

Independent: see Define whether User Types can Disable Alarms Independently in the Geo SCADA Expert Guide to Server Administration.


Disclaimer

Geo SCADA Expert 2020