ATTENTION: This section and associated topics apply to the Original WebX client only.
If you attempt to access your system from an Original WebX or XML client and it is unable to establish a connection, the web browser application that you are using will display a ‘connection failed’ message.
Original WebX and XML clients use the built-in Web Server to connect to the Geo SCADA Expert server. The settings for the Web server are configured using the Server Configuration Tool, see Web Server Settings.
If your web browser displays a connection failed message, it may be because:
- The user of the Original WebX or XML client has entered an incorrect port number in the Address field on the browser (if the default ports are not used).
- The network connection between the client PC and server PC is unavailable. This may be due to failed hardware or a temporary loss of connection. If you suspect that there is no network connection, please contact your network administrator.
- There is a firewall blocking the connection between the client PC and the server PC. If a firewall is being used between an  Original WebX or XML client and the web server, you need to configure it to allow the ports that are being used. For more information on configuring your firewall, please refer to the manufacturers’ documentation supplied with the firewall software or hardware.
            The default settings for Original WebX and XML clients with the Web Server are (http) 80 and (https) 443. 
- The configuration that enables the Original WebX and XML client to communicate with Geo SCADA Expert via a proxy server or proxy firewall is incomplete or incorrect. For example, the proxy settings in Geo SCADA Expert differ to those configured in the proxy application in which the actual port mapping occurs, or the mapping is configured incorrectly in that application. (This scenario only applies if your system uses a proxy server or proxy firewall between the Geo SCADA Expert Web server and Original WebX clients, and the Original WebX clients are set up to communicate with Geo SCADA Expert via the proxy.)
- A third-party web server on the Geo SCADA Expert server is using the ports that the Geo SCADA Expert web server is configured to use. For example, if the Apache web server is installed on the Geo SCADA Expert server and is using port 80, it will stop the Geo SCADA Expert web server from using port 80. In this situation, there are two possible solutions: - You can reconfigure the Geo SCADA Expert server so that the Geo SCADA Expert web server uses different ports for the connection with Original WebXOr: 
- You can reconfigure the third-party web server to use different ports.
 
- You can reconfigure the Geo SCADA Expert server so that the Geo SCADA Expert web server uses different ports for the connection with Original WebX