Install the Data Access Components on a Third Party OLEDB Client

A Third Party OLEDB client can only connect to a Geo SCADA Expert server’s if it has the Geo SCADA Expert Data Components installed. The Data Access components allow OLEDB applications to access your Geo SCADA Expert database. They also handle the communications between Geo SCADA Expert and the OLEDB client.

To install the Geo SCADA Expert Data Access components on a computer that runs Third Party ODBC application(s):


Disclaimer

Geo SCADA Expert 2020