Launch a ViewX Client on a Multi-Monitor Setup

You can configure a ViewX client to launch on a Multi-Monitor setup with specific interface components displayed on each monitor. By associating a Window Container with a particular monitor, you can manage the content the monitor displays.

You use a Startup Configuration File to define how many Window Containers are required by a Multi-Monitor setup, and the content that each displays (see XML Elements).

You can also use the Startup Configuration File to:

NOTICE

unexpected behavior OF APPLICATION

Startup Configuration files are intended only for use on ViewX clients that are required to launch Geo SCADA Expert on a Multi-Monitor setup, and/or have customized Window Container behavior.
Do not use Startup Configuration files on Virtual ViewX clients, as these clients only support a single monitor setup, and do not support the same customized behavior. Using a Startup Configuration file on such a client could result in unexpected behavior. (Startup Configuration files are not supported, and are ignored, on Original WebX clients.)
Failure to follow these instructions can result in inoperable equipment.

Disclaimer

Geo SCADA Expert 2020