The Primary Window Container is intended to display on the monitor that is the operational focus of a Multi-Monitor setup.
It is the only type of Window Container that supports the following ViewX interface components:
- File menu
- ViewX ribbon
- Status bar
- Tool windows (such as the Database Explorer and the Messages Window).