Geo SCADA Expert includes a series of default colors to denote different states, severities or system activities. Many of these colors can, if required, be changed so that they are more appropriate to your requirements. Geo SCADA Expert includes color palettes for:
- System Colors—Core and driver-specific colors that denote that an item is in a particular state, for example Overridden (see System Colors).
- Alarm Severity Colors—Colors that indicate whether, for instance, an alarm has been acknowledged or cleared (see Alarm and Event Severities in the Geo SCADA Expert Guide to Server Administration).
- State Colors—A non-alarm state that needs to be brought to the attention of operators. For instance, the fact that a pump is running. For information, see Defining a Custom State Color.