Define the Period of Forecast Data for which Geo SCADA Expert can Generate Limit Alarms

Use the fields within the Alarm Time Window section of the Forecast tab to specify the period of Forecast data for which Geo SCADA Expert is able to generate any limit alarms that are defined in the Alarm Limits section of the tab (above).



Disclaimer

Geo SCADA Expert 2020