Priority of Outstation Foreground Colors
This chart indicates which advanced driver outstation status takes precedence over another, and therefore which core system foreground color is assigned to an outstation at any particular time:
As such, if a PSTN outstation:
- Has valid configuration
- Is In Service
- Is not in alarm
- Does not have its alarm functionality disabled
- Does have its Dial In capability disabled (through use of the Disable Dial In pick action)
the outstation’s foreground color will be brown, by default, to indicate that Dial In is disabled on that outstation (unless a driver-specific state applies, which takes priority over the Dial In Disabled state). However, should Geo SCADA Expert dial out to the outstation, the outstation’s color will change to a flashing blue (the Outstation Connecting color) while Geo SCADA Expert establishes communications with that outstation. Once communications is established, the color will revert to the Dial In Disabled color (unless a driver-specific state and color takes priority), while Dial In remains disabled.
Further Information