Remove a Profile’s Vectors

To remove all of the vectors for a single day from a Time Profile and store a copy of those vectors in Window’s temporary storage ‘clipboard’:

  1. Display the required Time Profile(s) in Design mode.
  2. If the Time Profile(s) have a Weekly span, select the day of the week for which the vectors are to be deleted.

  3. Press both the CTRL key and the X key.
    The vectors are removed from the selected day of the week. A copy of the vectors is placed in the clipboard.

  4. Paste a copy of the vectors onto another day of the week on the same or another Time Profile, as required (see Use Copy and Paste to Copy a Profile’s Vectors).

To delete the vectors for a single day from a Time Profile, but not store a copy of those vectors:

  1. Display the required Time Profile(s) in Design mode.
  2. If the Time Profile(s) have a Weekly span, select the day of the week for which the vectors are to be deleted.
  3. Press the Delete key.
    The vectors are removed from the selected day of the week. The clipboard is not used during this function.

If you delete the vectors by accident, use the Undo feature to undo the deletion (see Use Undo and Redo).


Disclaimer

Geo SCADA Expert 2020