There are several ways to remove a single element from an array field:
- Select the element in the array field and select the Remove button.
- Select the element in the array field and then press the Delete key.
- Right-click on the element in the array field to display a context-sensitive menu, and then select the Remove option.
- Select the element in the array field and then press the Windows application key to display a context-sensitive menu. Select the Remove option.
If you want to remove several elements, a quicker, more efficient technique is described in Remove Multiple Elements from an Array Field.