To rename a database item using the Rename action:
- Display the Database Bar (see Display an Explorer Bar).
- Right-click on the database item in the Database Bar.
 A context sensitive menu is displayed.
- Select the Rename command from the relevant command group.
 The name of the database item is selected.
- Enter a new name to overwrite the existing name, or make amendments to the existing name. Remember to take into account any Naming Restrictions.
- Select another part of the ViewX display or press the Enter key to confirm the new name.