Using the Color Window

When you select the ... option on a pop-up color palette, the Color window is displayed (for information on accessing the color palette, see Using the Color Window to Define a Color).

To select a color from the Color window:

  1. Either:
    • Select a color from the Basic Colors palette.

    Or:

    • Select a color from the Custom Colors palette.

    Or:

    1. Specify a New Custom Color.
    2. Add the color to the Custom Colors palette.
    3. Select the new color from the Custom Colors palette.
  2. Select the OK button on the Color window.

Disclaimer

Geo SCADA Expert 2020