Field Types

You can add various types of field to a report. A summary of some of the types of field and how they are used in conjunction with Geo SCADA Expert is given below. For more information on field types and using fields in reports, see the documentation supplied with the Crystal Reports application.

To add any static text to your reports, you need to add a Text Object. You add a Text Object by using the Insert Text Object menu option or toolbar button. If you want to add specific information to a report, such as the report title or a page number, you may want to insert a Special Field, rather than static text.

The types of field that you may want to use in your reports include:

If the data that you want to include in your reports contains calculations, you may want to consider using Data Grids. Data Grids are ‘custom’ tables that you can configure within Geo SCADA Expert. Geo SCADA Expert can perform a variety of calculations on the data in a Data Grid and display the results of those calculations in the report. For further information, see Configuring Data Grids in the Geo SCADA Expert Guide to Core Configuration. For an example of how a Data Grid can be used in a report, see Embedded Data Grid Content.


Disclaimer

Geo SCADA Expert 2020