Define the Direct Communications Re-establishment Delay
            Use the Delay after closing line before starting direct comms field in the DNP3 Master section of the tool to specify a delay that allows a DNP3 outstation sufficient time to establish direct communications before receiving any messages:
                
            
This delay applies to direct outstations that have been using PSTN fallback to communicate with the server.