Configure the ER I/O Properties
            Use the fields on the ER I/O tab of the DNP3 SCADAPack ER IO Form to configure these card-specific properties:
                
            
- Outstation—Use to Specify the SCADAPack Outstation with Which the I/O is Associated.
 - Card Type—Use this combo box to specify the type of input or output card that this particular SCADAPack ER IO item represents.
 - Slot—Use this combo box to specify the slot location (Slot 1 to Slot 13) of the I/O card.