Specify how the SCADAPack Outstation Handles any Pulse Action Events
            The RTU Event property applies to DNP3 SCADAPack Pulse Actions that have a Point Type other than Physical Output, and a Point Data Class of Class 1 Event, Class 2 Event, or Class 3 Event (see Configure Common Properties of DNP3 SCADAPack Points).
                
            
- RTU Event—Use this combo box to specify whether the SCADAPack E outstation just stores each Pulse Action event, or whether it immediately generates an unsolicited message (see Specify Whether a Class n Event Triggers an Unsolicited Message).