Specify the Outstation Type and Port Configuration Properties
            Use the fields on the Outstation Type tab of each DNP3 SCADAPack E Outstation Form to:
- Specify the Outstation Type
 - Configure the Properties of the Individual Ports
 - Configure the SCADAPack ER-P620 IRIG Mode (applies to SCADAPack ER-P620 outstations only).