Access the Database Schema
You can use most up-to-date HTML5-compatible web browsers to access the Geo SCADA Expert Database Schema. You can then use the Geo SCADA Expert Database Schema to locate information about the classes.
The List all <Type of Database Item> Objects links in the database Schema provide access to Original WebX (providing that the Original WebX server is installed on your Geo SCADA Expert server machines). You need to use the 32-bit version of Internet Explorer to access Mimics and other displays that use ActiveX controls in Original WebX (other browsers are not supported).
To access the Geo SCADA Expert Database Schema:
- Open a web browser on any PC in the network.
- In the Address field, overwrite any existing address with:
http://<server name>:<web server port>/Schema
Where:
-
<server name>is the name of one of your Geo SCADA Expert servers <web server port>is the HTTP port number that is defined in the WebX section of the Geo SCADA Expert Server Configuration Tool (see Define the Ports Settings for WebX Clients in the Geo SCADA Expert Guide to Security).
Do not enter the angle brackets <>.
Alternatively, if you are using the server PC and it uses port 80 for the web server's port, you can enter:
http://localhost/Schema
-
- Press the Enter key or select the Go button.
The Geo SCADA Expert Database Schema is displayed.