Aggregates Section

In the Database Schema, the Aggregates section shows information about the Aggregates of the class (aggregates are special types of class that act as an extension of another class).

Example:

The Aggregates section for the CGenericModbusOSPSTN class shows information about the aggregates of the CGenericModbusOSPSTN database class.

For each Aggregate of the class, the following information is shown:


Disclaimer

Geo SCADA Expert 2020