Document Scope
The Geo SCADA Expert Guide to the Database provides information about the structure of the Geo SCADA Expert database. It also explains how to use the Geo SCADA Expert Database Schema to locate specific information about the database tables.You may need to access this information when:
- Creating Mimics (for animations, pick action menus, embedded Lists, and so on)
- Creating Trends (trace source)
- Creating Reports
- Creating Logic programs (function block diagrams, structured text programs, and so on)
- Customizing the Alarm Banner (adding extra columns, and so on)
- Adding or modifying extra fields in the database
- Using external applications to access the database (via ODBC, OPC, SOAP, or Automation).
Intended Audience
This guide is designed to help users understand the structure of the Geo SCADA Expert database. The information it contains may be useful to engineers who are responsible for configuring:
This guide also provides information about the Configuration Change CRC feature that can be used to help to detect whether an item's configuration has changed (see Understand Configuration Change CRCs).
If you are unfamiliar with the structure of the database and how the Geo SCADA Expert Database Schema works, we suggest that you:
- Familiarize yourself with the structure of the database (see Understanding the Database).
- Learn how to use the Geo SCADA Expert Database Schema to view information about different tables (see Working with the Database Schema).