Create a Mimic on which to Display the Point

To create and populate a Mimic:

  1. Create a Mimic.
  2. Use the Database Bar to locate the EtherNet/IP Analog Point that you created earlier in this tutorial.

  3. Drag-and-drop the EtherNet/IP Analog Point onto the Mimic.
    A context-sensitive menu is displayed.
  4. Select the Value option.
    A further menu is displayed.
  5. Select Formatted Value option.
  6. Save the Mimic.
  7. Put the Mimic into Run mode.
  8. For information on creating and configuring a Mimic, see Geo SCADA Expert Guide to Mimics.


Disclaimer

Geo SCADA Expert 2020