Create a Ladder Diagram Database Item

Each Ladder Diagram needs to be represented in the Geo SCADA Expert database by a Ladder Diagram item. When you have created a Ladder Diagram item, you can access its Edit feature which allows you to create the Ladder Diagram program.

To create a Ladder Diagram database item:

  1. Display the Database Bar (see Display an Explorer Bar).
  2. In the Database Bar, right-click on a system, Group, or Group Template to display a context sensitive menu.
  3. Select the Create New option, then the Logic option, then the Ladder Diagram option from the context sensitive menu.
    A new Ladder Diagram item is added to the system, Group, or Group Template. It is selected automatically, ready for you to enter its name.
  4. Enter a suitable name for the Ladder Diagram then press the Enter key or select another part of the interface.

Now that you have created a Ladder Diagram database item, you can edit it (see Edit a Ladder Diagram).


Disclaimer

Geo SCADA Expert 2020