DELETE

Function Name

DELETE

Description

Removes a defined number of characters from an input string and outputs the remainder of the string.

Arguments

IN {STRING}

The IN input is a string input. It has a specified number of characters removed by the DELETE function then its remaining characters are used as the output.

L {INT}

The L input defines the number of characters that will be removed from the IN input for the output string.

P {INT}

The P input defines the position of the character in the string where the deletion starts (1 is the first character, 2 is the second character, 3 is the 3rd character and so on).

For more information on the data types for the inputs and outputs, see Data Type Hierarchy.

Returns

Output {STRING}

The output is the characters remaining from the IN string (IN string - L characters starting from P).

Example:

Function Block Diagram - DELETE:

In this example, the IN is ALARMCONDITIONS, the L is 10, the P is 6 and so the output is ALARM. 10 characters have been deleted from the 6th character (inclusive) onwards—CONDITIONS has been removed.

ST Program - DELETE:

To use a DELETE function in an ST program, you need to use this syntax:

Output := DELETE (IN, L, P);


Where Output, IN, L, and P are defined as variables earlier in the ST program.

Alternatively, you can use the following syntax:

Output := DELETE (IN:= 'ALARMCONDITIONS', L:= 10, P:= 6);

Where the 'ALARMCONDITIONS', 10 and 6 values are the input values (in this case, they are the same values as used in the Function Block Diagram example above).


Disclaimer

Geo SCADA Expert 2020