DIVTIME
Function Name |
DIVTIME |
---|---|
Description |
Provides a time interval output that is the result of a time interval input divided by an integer input. |
Arguments |
Input 1 {TIME} Input 2 {INT} For more information on the data types for the inputs and outputs, see Data Type Hierarchy. |
Returns |
Output {TIME} The output is the result of Input 1/Input 2. |
Example:
Function Block Diagram - DIVTIME:
A DIVTIME function has 2 inputs (in this case, the inputs are constants):
- Input 1 is a time value and is set to 59h (59 hours)
- Input 2 is an integer and is set to 4.
The DIVTIME function divides 59 hours by 4 to provide the output of 14h45m (14 hours and 45 minutes).
ST Program - DIVTIME:
The syntax for a DIVTIME function in an ST Program is:
Output := DIVTIME (Input 1, Input 2)
Where Output, Input 1 and Input 2 are defined as variables earlier in the ST program. Each input is separated by a comma. Input 1 is a Time value, Input 2 is an integer value and the Output is a Time value.