DT_TO_TOD

Function Name

DT_TO_TOD

Description

Converts a Date and Time input into a Time of Day output (the output will not include a date).

Arguments

Input 1 {DATE_AND_TIME}

For more information on the data types for the inputs and outputs, see Data Type Hierarchy.

Returns

Output {TIME_OF_DAY}

The output is the result of Input 1 - the Date supplied by Input 1.

The DT_TO_TOD function works in a similar way to the DT_TO_DATE function except that it determines its output by using Time part of the Date and Time input instead of the Date part. For ST Programs, a similar syntax is used:

Output := DT_TO_TOD (Input 1)


Disclaimer

Geo SCADA Expert 2020