Associated with: ST Programs, Function Block Diagrams, Ladder Diagrams
Security permission required to access this pick action: Configure
Use the Execute action to trigger a Logic program manually. When you select the Execute action, the Logic program runs and the functionality provided by the program is applied. For example, if you have a Logic program that calculates the average value of two input points, when you select its Execute action, the program will read its inputs and calculate the average value at that time.
You can only select the Execute action if the Logic program’s execution status is set to Enabled (see Enable Execution) and the Logic program is configured to allow manual execution (see Define whether a Logic Program can be Executed Manually).