MOD

Function Name

MOD (Modulo)

ST Operator

MOD

Description

The output is the modulo result of a division (the remainder of a division). For the MOD function, Input 1 is divided by Input 2 and the remainder is the output. In Function Block Diagrams, Input 1 is the top input and Input 2 is the bottom input.

Arguments

Input 1 {ANY_INT}

Input 2 {ANY_INT}

For more information on the data types for the inputs and outputs, see Data Type Hierarchy.

Returns

Output {INT}

The Output = The remainder of Input 1 / Input 2

Example:

Function Block Diagram - MOD:

Input 1 is 5 and Input 2 is 2. This means that the MOD function provides an output of 1 as 5/2 = 2 with 1 remaining.

ST Program - MOD:

The MOD function outputs the remainder from Input 1 divided by Input 2.

Output := MOD (Input 1, Input 2);

Where Output, Input 1 and Input 2 are defined as variables earlier in the ST program. In this case, let's assume Input 1 is 10 and Input 2 is 3. The MOD function returns 1 as 10/3=3 with 1 remaining.


Disclaimer

Geo SCADA Expert 2020