MULTIME
Function Name |
MULTIME |
---|---|
Description |
Outputs a time interval value that is the result of a time interval value multiplied by an integer value. |
Arguments |
Input 1 {TIME} Input 2 {INT} For more information on the data types for the inputs and outputs, see Data Type Hierarchy. |
Returns |
Output {TIME} |
Example:
Function Block Diagram - MULTIME:
A GT function has 2 inputs (in this case, 2 constant values). Input 1 is has a time value of 59 hours (TIME#59h) and Input 2 has an integer value of 4. The MULTIME function outputs a time value of 9d20h as this is the result of 59 hours multiplied by 4.
ST Program - MULTIME:
The syntax for a MULTIME function in an ST Program is:
Output := MULTIME (Input 1, Input 2)
Where Output, Input 1 and Input 2 are defined as variables earlier in the ST program. Input 1 is a time value, Input 2 is an integer value, and the Output is a time value.