OPEN_FILE_EX
Function Name |
OPEN_FILE_EX |
---|---|
Description |
Opens a file on disk in binary or text mode. The file can be used to store a value, text etc. When a file has been opened, data can be written to it by using the WRITE_FILE function (see WRITE_FILE) or WRITE_FILE_BYTE function (see WRITE_FILE_BYTE). |
Arguments |
FILENAME {STRING} The FILENAME string defines the name of the file that is to be opened. APPEND {BOOL} Controls whether data is added to the end of the file (True) or the existing data is overwritten (False). BINARY {BOOL} Controls whether the file is opened in text mode (False) or binary mode (True). For more information on the data types for the inputs and outputs, see Data Type Hierarchy. |
Returns |
FileID {UDINT} Returns the FileID of the file. The FileID is used to identify the file when writing and closing. |
You should only use the OPEN_FILE_EX function in ST Programs.
Example:
ST Program - OPEN_FILE_EX:
To use an OPEN_FILE_EX function in an ST program, you need to use this syntax:
FileNumber := OPEN_FILE_EX( FILENAME, APPEND, BINARY );
Where FileNumber, FILENAME, APPEND, and BINARY are variables that are declared earlier in the ST program. The FILENAME variable has to be a string, and the APPEND and BINARY variables have to be Booleans. The FileNumber variable will be used to store the FileID that is returned when the specified file is opened.