OPEN_PORT
Function Name |
OPEN_PORT |
---|---|
Description |
Opens a serial port. When a port is open, data can be written to it by using the WRITE_FILE function (see WRITE_FILE). |
Arguments |
SPEC {STRING} A string input that is a serial port specification, for example 'COM1,9600,8,N,1,NONE'. For more information on the data types for the inputs and outputs, see Data Type Hierarchy. |
Returns |
FileID {UDINT} Returns the FileID of the file that is to be used when the port is writing or closing. |
Example:
ST Program - OPEN_PORT:
To use an OPEN_PORT function in an ST program, you need to use this syntax:
PORT := OPEN_PORT( 'COM1,9600,8,N,1,NONE' );
Where PORT is a variable declared earlier in the ST program.