TAN
| Function Name |
TAN |
|---|---|
| Description |
Converts a REAL or LREAL input into a tangent value that is the output. The tangent value is also a REAL or LREAL. |
| Arguments |
Input 1 {REAL or LREAL}. This value is in radians. For more information on the data types for the inputs and outputs, see Data Type Hierarchy. |
| Returns |
Output {REAL or LREAL} |
Example:
Function Block Diagram - TAN:
In this example, the input of 5 is provided by the CurrentValue property of a point. The TAN function converts the value into a tangent value of -3.38051500624659.
ST Program - TAN:
The syntax for a TAN function in an ST Program is:
Output := TAN (Input 1);
Where Output and Input 1 are defined as variables earlier in the ST program. The Input 1 variable represents a REAL or LREAL type of value (the output is the same type of value as Input 1).